Other Parts Discussed in Thread: TCA9548A, TCA9545A, LDC1614
Hi,
I am using a TCA9548A (on a DFR0576 Gravity board).
I can write to and read from the control register without any issues (the read data reflects the write data, so I know it is been written correctly).
I also checked in on a scope and the waveforms look correct.
The master I am using is a National Instruments NI-8452 (I have disabled the pullups on it as the DFR0576 board has pullups to 3V3 on both the input channel and all the 8 output channels).
However when I enable any of the output channels I don't see anything appear on the output.
I have disconnected the I2C devices from the TCA9548A outputs but still don't see any activity on the output lines. They remain at 3V3.
I had also tried the TCA9545A (4 channel part) earlier with the exact same symptoms.
I am baffled as to what is the cause. Any help, suggestions would be greatly appreciated.
Kind regards,
Conor.