This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN55HVD233-SP: SN55HVD233-SP CAN transceiver for space application

Part Number: SN55HVD233-SP


Hello,

I am interesting to use SN55HVD233-SP CAN transceiver (space grade) but in ordering option is presented some other part  5962L1420901VXC. What difference4 between parts and what actually I should to define in data base for ordering?

Thanks,

Semyon

  • The Standard Microcircuit Drawing is a vendor-independent datasheet. The SMD is linked from the product web page; it explains the structure of the PIN in section 1.2.

    You would order both of them. HVD233HKX/EM is an engineering sample; footnote 2 in section 3 of the datasheet says:

    These units are not suitable for qualification, production, radiation testing or flight use. Parts are not warranted for performance over the full MIL specified temperature range of –55°C to 125°C or operating life.