What are the pros and cons of using nWKRQ vs nINT for waking the host MCU. We will implement the ISO 11898-2:2016 WUP. I see the timing nWKRQ vs nINT is a bit different in the wake event, which doesn't matter to us. We already have nINT connected, but host MCU pins are scarce so we would like to avoid nWKRQ unless needed. The nINT host MCU interrupt routine will change dependent on the mode/state it's in. Are there some scenarios where nWKRQ could prove beneficial or absolutely necessary?