Part Number: DS90UB933-Q1
1; When the contact discharge and air discharge test (4/6KV) is carried out on the screw position of the product, the image will flicker with probability. If the product extension wire is shortened, the probability will be reduced. Do you have any good suggestions?
2: In the failure of the product, through which registers can be determined whether the input is caused or the output is caused by the failure, which can be sent out to know this information?
3; At present, it is known that electrostatic conduction to the camera inside the ground, causing probability failure