Part Number: DS90UB913A-CXEVM
Other Parts Discussed in Thread: ALP
The manual for the EVM boards states the boards can be used with other than the pair that shows up in the Analog launchpad. So a 913 has the 914 partner, the 954 has the 953 partner. How does the partner get updated for the interface being used. Specifically a 913A and 954 that is allowed per the manual for the DS90UB954 EVM if the power is not over coax and 5 V is on the 913 board.