Part Number: TCA9511A
Other Parts Discussed in Thread: TCA4307, TCA9509
Hello Sir:
We are searching hot swapable with 2 bit level transfer.
Such as NXP, PCA9512A, or ADI LTC4315.
Please let us know your recommendations.
Thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Clemens:
We need has level shift function, likes PCA9512A and LTC4315.
But TCA9511A and TCA4307 has no this function.
Please recommend others for us.
Thanks a lot.
The I²C signals can be pulled up to a voltage higher than VCC.
There is no hot-swappable I²C buffer with two separate supplies.
Hi Statham,
As Clemens has mentioned, we do not offer a hot-swappable buffer with dual supplies specifically for level-translation. TCA9511A or TCA4307 would be a good device choice when compared to the PCA9512A or LTC4315.
While our hot-swappable buffers do not have dual supplies specific for level-translation, I agree with Clemens comments on having the I2C signals being pulled up to a voltage higher than VCC.
What voltage level is the customer trying to translate to? 1.8V to 3.3V, 3.3V to 5V, etc?
Regards,
Tyler
Hi Tyler:
Sadly, customer application are only 3.3V or 1.8V to 3.3V.
If operate on 1.8V to 3.3V application, which means both TCA9511A and TCA4307 can not be used on their product.
Am I right?
Looking forward your feedback.
Thanks a lot.
Hi Statham,
The TCA4307 and TCA9511A would work with the voltage ranges of 1.8V / 3.3V / 5V, but they do not conduct proper level translation. You could try using the TCA9509 which is a buffer with dual supply for level translation, however, this device does not support hot-swap capability. The hot-swap portion would have to be done with external components in addition to the TCA9509.
Regards,
Tyler