This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1431-Q1: can we provide separate VCC to microcontroller and not use VCC from SBC chip

Part Number: TLIN1431-Q1

HI team,

I am intent to provide separate power rails to Microcontroller ( 3.3V) and not using TLIN1431-Q1 VCC power rail from internal regulator.

I am confuse here, because in application Microcontroller VCC is connected with LIN SBC chip VCC.

Also I saw somewhere in the application that for channel expansion , Microcontroller vcc is separate. But I do not want to use channel expansion.


Please suggest how this can be done .

Thanks in Advance.

Regards,
Satish