This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848K: Resistor value for weak internal pulldown resistor

Guru 19685 points

Part Number: DP83848K

Would you let me know the range of resistance values for the weak internal pull-down of PHYAD1 to PHYAD4?

If there is no nominal value, calculate the resistance value of the weak internal pull-down using the following concept, Is this correct?

・There is a description "A 2.2-kΩ resistor should be used for pulldown or pullup to change the default strap option"

・According to the specified values, Vcc=3.3V, VIH(min)=2V

 Considering that 2V (or more) of VIH (min) can be guaranteed with an external 2.2kΩ pull-up

 ⇒R=2.2kΩ×(2V÷(3.3V-2V))≒3.384kΩ(min)

Best regards,

Satoshi