Part Number: DS90UB935-Q1
Hi E2E,
The connection to DS90UB935TRHBRQ1 is DS90UB954TRGZRQ1.
In the ESD air discharge and contact discharge, there will be video delay when the voltage is above 4kV.
At this time, the IPS input signal to DS90UB935TRHBRQ1 is continuous and without abnormality.
The details are confirmed as follows:
1, a single ESD air discharge test to the product as shown in the attached video(DS90UB935TRHBRQ1-ESD) about 5s test stuck.
2. When the continuous test is applied, the MCU determines that the output signal of DS90UB935TRHBRQ1 is abnormal and takes the initiative to restart the whole camera.
Through the above phenomena, it is seems that the abnormal output of DS90UB935TRHBRQ1 in ESD test leads to the screen delay.
(NOTE:The SCH & PCB layout are non-public and can only be shared with TI)