Part Number: PCA9515A
Other Parts Discussed in Thread: PCA9515,
First question: What is the value of the internal pull up resistor to VCC on the 9515A/B parts? Would a control line with a 10K pulldown resistor be enough to keep the device "disabled".
Second Question: When disabled, the two sides are completely isolated correct? ie. not traffic/current passes through the part?
Third Question: My application is a follows: I have an always on low power consumption section (+3.3V) of the board with I2C peripherals. Occasionally, I need to power on a high power consumption section of the board (+3.3V) w/ I2C peripherals to perform some functions and then power down. Both sides are +3.3V.
Is the PCA9515A/B the correct part to bridge the two sides? Another more appropriate device? The PCA9515 will always be powered, but disabled (question 1) most of the time.
Thank You
Paul