This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1: How to connect for unused GPIO??

Part Number: DS90UB949-Q1

Hello team,

While I checked my customer schematic for 949, I see no connection for unused pins as below table.

But I don't have any guide from datasheet if they can be leave as floating.

Could you pls help check it??

PIN

I/O, TYPE

DESCRIPTION

DES 940

SER 949 connection

NAME

NO.

D_GPIO0 / MOSI

8

IO, LVCMOS
IO, LVCMOS

HS GPIO0. Shared with MOSI
SPI Master Out Slave In. Shared with D_GPIO0

not use

??

D_GPIO1
MISO

10

IO, LVCMOS
IO, LVCMOS

HS GPIO1. Shared with MISO
SPI Master In Slave Out. Shared with D_GPIO1

not use

??

D_GPIO2
SPLK

11

IO, LVCMOS
IO, LVCMOS

HS GPIO2. Shared with SPLK
SPI Clock. Shared with D_GPIO2

not use

??

D_GPIO3
SS

12

IO, LVCMOS
IO, LVCMOS

HS GPIO3. Shared with SS
SPI Slave Select. Shared with D_GPIO3

not use

??

SDIN / GPIO0

4

I, LVCMOS
IO, LVCMOS

Master Mode I2S Data Input. Shared with GPIO0
BCC GPIO0. Shared with SDIN

not use

??

SWC / GPIO1

5

O, LVCMOS
IO, LVCMOS

Master Mode I2S Word Clock Output. Shared with GPIO1
BCC GPIO1. Shared with SWC

not use

??

I2S_DC
GPIO2

37

I, LVCMOS
IO, LVCMOS

Slave Mode I2S Data Input. Shared with GPIO2
BCC GPIO2. Shared with I2S_DC

not use

??

I2S_DD
GPIO3

38

I, LVCMOS
IO, LVCMOS

Slave Mode I2S Data Input. Shared with GPIO3
BCC GPIO3. Shared with I2S_DD

not use

??

I2S_DB

GPIO5_REG

36

I, LVCMOS

IO, LVCMOS

Slave Mode I2S Data Input. Shared with GPIO5_REG

General-Purpose Input/Output 5
Local register control only. Shared with I2S_DB

not use

??

I2S_DA

GPIO6_REG

35

I, LVCMOS

IO, LVCMOS

Slave Mode I2S Data Input. Shared with GPIO6_REG

General-Purpose Input/Output 6
Local register control only. Shared with I2S_DA

not use

??

I2S_WC

GPIO7_REG

33

I, LVCMOS

IO, LVCMOS

Slave Mode I2S Word Clock Input. Shared with GPIO7_REG

General-Purpose Input/Output 7
Local register control only. Shared with I2S_WC

not use

??

I2S_CLK

GPIO8_REG

34

I, LVCMOS

IO, LVCMOS

Slave Mode I2S Clock Input. Shared with GPIO8_REG

General-Purpose Input/Output 8
Local register control only. Shared with I2S_CLK

not use

??

MCLK

16

IO, LVCMOS

Master Mode I2S System Clock Input/Output

not use

??

Thank you.