Part Number: DP83869HM
Hi support team!
Im using the DP83869HM, project in design stage and i want to clarify some points about RESET_N pin.
It is clear that RESET_N shall be held low for minimum 200ms after the last supply power up.
In my design PHY part will be started automatically and uP won't be able to control it, so i want to use the option proposed in DS (simple RC curciut). But im confused about RESET_N pull-up inside the IC.
In the DS, table 7-1 RESET_N pin type is not PU, its just empty, but in the tables 7-2, 7-3, 7-4 i can see that the pin is PU or PD.
So there are the questions:
1) Is there a pull for RESET_N pin inside the chip? If so, what the purpose of external 100Ohm in RC curciut? Current will be limited more by internal pull up, because it weak i guess
2) If so, does RESET_N pull type depends on mode used?
3) What the inside pull-up typ. resistance value?
Thanks in advance,
Ivan