Part Number: TSER953
Other Parts Discussed in Thread: TDES954
Hi Team,
customer is working with TSER953 & TDES954 on a medical product.
They have a set-up with two EVMs.
The two evaluation boards are connected with a Fakra cable. However, the Fakra connector is not very common in industry, but in the automotive industry. It is difficult to get a cable with the appropriate length and characteristics (drag chain).
They will probably use a different connector, for example SMA.
They do not have an indication of the maximum attenuation of the cable between the serializer and the deserializer if the functionality is still guaranteed.
Could you please help answering this question?
BR,
Stefan