Part Number: TDP158
I am using the TDP158RSBEVM board to convert DisplayPort to HDMI for one of our modules, but to test I am using a Viewsonic monitor with a HDMI input.
My GPU shows "DVI" for the connector type in the control panel. I use a different DP to HDMI convertor and the connector type shows up as "HDMI".
Is there a setting for this on the eval board or with use of the TDP158? I see the DP connector has pin 13 (DP_CAD) pulled HI. The DisplayPort specification shows this pin as CONFIG1.
See figures below, the first one is the eval board which yields "DVI", the next one is the other adapter which is "HDMI"