Part Number: AM26LV32E-EP
What is the output voltage level when Vcc = 3.3V and Vinputs are in the range +5V. Whether the output will follow Vcc supply voltage or Vinputs.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM26LV32E-EP
What is the output voltage level when Vcc = 3.3V and Vinputs are in the range +5V. Whether the output will follow Vcc supply voltage or Vinputs.
The purpose of a differential receiver like this is to convert any input signal inside the valid common-mode range (±7 V) into a proper logic signal at the output. As shown by the VOL/VOH specifications, the output voltage is determined by VCC.
Hi Balaram,
Outputs are bounded by VCC and GND - Clemens analysis is correct. Essentially the differential receiver will convert the differential voltage to a logic level bounded by VOL/VOH (if the load is high impedance - and you are only drawing 100uA or less then VOL = 0.1V (max) and VOH = VCC - 0.1 (max) - more current output will attenuate the output voltage).
Please let me know if you have any other questions!
Best,
Parker Dodson