Part Number: DS125BR111
Hi Experts,
I would use DS125BR111 for SAS-3 interface redriver and am consider setting. Now I have some questions about this device. I use it on pin-mode as ENSMB=0.
1) I set the EQA0/EQB0=1 (LEVEL4), VODA_DB/VODB_DB=0 and VOD_SEL=1 as recommended setting. In this case, will all ranges of SAS-3 are covered, i.e. there is no problem? For example, when I put this device with short cable near output and loss is only a few dB, will it work fine?
2) Block diagram shows Equalizer, Pre-driver, Driver. What are the functions of Pre-driver and Driver? Are they only pure amplifiers or do they work for adjusting output to specific level according to SAS-3 format?
Best regards,
Tetsu