Part Number: TUSB8020B
Hi, expert
Customer wants to test the USB2.0 & USB3.0 signal quality and eye diagram, just like below.
要求测试USB接口的USB2.0和USB3.0信号及眼图,如下图所示:
测试方法:在USB插座插入测试工装(就是一个USB公头转出2条馈线/4条馈线直接接到示波器的工装连接器)从CPU强制发送USB2.0/3.0报文,经过HUB转到USB插座,在进入工装的馈线传输到示波器,从而进行对应的USB接口的信号质量测试。
Method: Connect the test tool to the USB connector (the test tool convets the USB signal into OSC probe interface) Send message from CPU, through the USB HUB-TUSB8020B and go to the USB connector, at last to the OSC for measurement.
当前进展:
Right now, from CPU pins, the message can be seen.
目前,已经确认从CPU处已经可以强制发出USB2.0和USB3.0的报文了,如下图单端探头所探测到的,单端探头和示波器采样率不够可能抓的波形难以抓到全貌,正式测USB有更好的示波器+工装可以抓全差分对的信号:
USB2.0:

USB3.0:

However, the message cannot be seen after the HUB. Please help check what the issue is. Thanks.
但是对应的报文送入HUB之后,在hub的输出端无法探测到对应的USB报文。目前请予以解决此问题,完成HUB对强发报文的转发传递: