Part Number: THVD1410
Other Parts Discussed in Thread: THVD1452, THVD1424
Hi
we are using the THVD1410 device in making a audio conference system
running the device at 3.3VDC.
Termination at the o/p (across A B pins) is of 120 ohm
Conference system is like:
1 chairman unit ..and multiple (25 units ) as delegate units.
Output from Chairman unit (AB output)....is connected to Delegate unit (via RJ45 CONNECTOR, CAT 6 CABLE)
When we are sending command from Chairman unit to delegate unit ..it is going ..and we are receiving it back (delegate to chairman unit)
2 way communication is happening.
The problem:
Now if we are connecting ..second Delegate unit (2nd delegate unit is connected from first delegate unit.....via RJ45, CAT 6 cable)
than command from chairman unit t0 delegate unit 1 and 2 is going....but when receiving the command from 2nd delegate unit ..we are getting lot of garbage data .
one to one units are working OK...WHEN CONNECTING MANY IN PARALLEL....DATA IS NOT PROPER ..
Looking for suggestions.
rgds
yogesh singhal