Part Number: DS16F95QML
Is there a specification for the minimum or maximum input rise time of this device, for both the single ended and differential inputs? Looks like only the output transition time is specified in the datasheet.
I also see that the enable input voltage pin has an absolute maximum voltage of 5.5V, would the DE pin also tolerate -0.5V as a limit for undershoot? Would the DI pin have the same specifications?