Part Number: TUSB1002A
Hi Team,
Please advices me on my question.
Which EQ level do you recommend for the RX2 (Receptacle to Host Path).
On the RX1 path (Host to receptacle Path ) the insertion loss is predictable.
However, on the RX2 (Receptacle to Host path), the insertion loss is unpredictable.
Because, different length of cables may be attracted to the receptacle.
If you set the high degrees EQ level may case over equalization against a short cable.
In contrast, low degrees of EQ setting may case under equalization against a long cable.
Mita