Part Number: TUSB1002A
Hi Expert,
Can TPS1002A P2P/B2B Parade PS8811? if yes, do we have co-design guideline can share to me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
PS8811 is a 4.2×4.2 mm 36-pin QFN Package while TUSB1002A is a 4x4 mm 24-pin QFN Package, the two do not have the same package.
Thanks
David