Part Number: DP83869HM
Hi,
I have some questions related to the pin states tables (7-2 to 7-4) and the pin function table 7-1 and about the general interpretation of the column PULL/HI-Z in table 7-2 to 7-4.
Is it correct, that this column PULL/HI-Z shows the internal configuration of the pin in the respective mode?
Why is, e.g. for pin INT_N/PWDN_n, the type column in table 7-1 empty, but in table 7-2 column PULL/Hi-Z we always have a PD, OD-PD? Shouldn't this pin be WPU in table 7-1, then? What is the difference between PD and OD-PD? Because we have here a PU in reset state, can I leave the pin open if I do not use the power down function?
Also for Pin 22, JTAG_TDO/GPIO_1, there is no info in table 7-1 that this is also a strap pin? Same for pin 23, JTAG_TMS / SUPPLYMODE_SEL.
Also for JTAG_TMS / SUPPLYMODE_SEL, for all modes we have PU in table 7-1 to 7-4, but in chapter 11 it is stated that this pin MUST be pulled high for triple-supply mode. Why, if we have internal PU?
Thank you for clarification.
Regards, Betty