Part Number: DP83640
Other Parts Discussed in Thread: DP83630, DP83869
Hi,
We need the IEEE 1588 PTP PHY, that we search the DP83640 is the 10M/100M PHY in TI website, please kindly advise if there are any 10M/100M/1000M PTP PHY promotion, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zhang Liang,
We also have the DP83630 which supports IEEE 1588 PTP at 10M/100M.
We do have a few devices which support SFD/SOF(Start of Frame Detection) which generate a signal when Start of Frame is detected. This is helpful for the MAC to eliminate the inaccuracy in time stamping caused due to the PHY. This is a feature which will be of a little help for MAC which runs the complete 1588 protocol.
Here are devices that support SFD/SOF:
DP83867 - 10/100/1000M
DP83869 - 10/100/1000M
DP83822 - 10/100M
Best regards,
Melissa