Other Parts Discussed in Thread: DS90LV012A, DS90LV011A, DS90LT012A, DS90LV028A, DS90LV027A, THVD1450, SN65LVDT41, DS90UA101-Q1
I'm looking at sending around 50 Mbps of data over a cable about 3 ft in length. None of the MCU have UART that can go that speed, so I am starting to look at some SERDES chips that can transmit over something like LVDS.
It looks like the only chips TI offers are FDP-Link. I'm not familiar with FDP-Link yet, but it appears that this is meant for video. Is there any reason this couldn't just be used for arbitrary data? Is there any better protocol? Minimizing the number of wires is important, and it looks like you can also do power over a data line, which would be great. These serializers and deserializers also seem very power-hungry.