Help confirm whether TI's TCAN1145 meets the following requirements:
1. Compatible with SAE J2284-3 standard?
2. Whether it meets the requirements in the figure below?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Help confirm whether TI's TCAN1145 meets the following requirements:
1. Compatible with SAE J2284-3 standard?
2. Whether it meets the requirements in the figure below?

Hi Xiaofu,
1. The SAE standards for CAN are high-level ECU requirements that impact the system as a whole. Generally they are not referencing transceiver requirements directly. These standards reference the ISO 11898-2 CAN physical layer standard for CAN transceivers which the TCAN1145 is compliant with.
2. Yes, the bit rate tolerance spec for this device is specified in the datasheet over all periods and bit transitions.
Let me know if you have any more questions.
Regards,
Eric Schott