Part Number: DS90UB940-Q1
Hi,
Whether DS90UB940 could support only RNI1 single port receive data and DSI port 0 output data?
There is no info for this configuration? if Yes, how to configure 940?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB940-Q1
Hi,
Whether DS90UB940 could support only RNI1 single port receive data and DSI port 0 output data?
There is no info for this configuration? if Yes, how to configure 940?
Hi Shuang,
Does your input need to be on RIN1? Can it be on RIN0? Typically for a single lane input on the 940, RIN0 is used.
To configure:
-the input is automatically configured based on 1 or 2 lane input, but you can also use register 0x34 to choose the mode of operation.
-the CSI outputs are configured using MODE_SEL0 and MODE_SEL1. I have included a screenshot of Table 7 and Table 8 from the datasheet that contain helpful information. MODE_SEL0 controls how many data lanes and number of ports the output uses and MODE_SEL1 controls which CSI port you use.

Best,
Holly Roper