This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9555: The I/O port can be read as a power-on reset (input state when the power is turned on), but in actual use it seems to be in the output state when the power is turned on

Guru 12235 points
Part Number: PCA9555
Other Parts Discussed in Thread: TCA9535

Hi, 

On the data sheet, the I/O port can be read as a power-on reset (input state when the power is turned on), but in actual use it seems to be in the output state when the power is turned on. (The LED to which the port is connected is lit.) Since there are discrepancies with the description in the datasheet, could you give us your opinion on possible causes?

Thanks,

Conor