Part Number: TCAN1146-Q1
Hi TI Team,
We have CAN bus network where we are using TCAN1146s with 5MBps data transfer mode, while other device connected on device is having 2Mbps CAN FD support. What issue we may have on the bus. Device supporting 2Mbps will ignore data transfer at speed of 5mbps. It would be same like classical CAN device connected on CAN FD network.
It is like for CAN FD bus network, all devices(transceiver) should support same data speed or different speed CAN FD device connection is ok.
This is required to inform other supplier should provide particular speed support for CAN FD ECUs.
Regards
Manoj A