Part Number: DS250DF230
//Set Data Rate
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS250DF230
Hi,
The DS250DF230 relies on CDR lock in order to generate PRBS data. In order to generate 10.3125 Gbps PRBS signal, you will need a 10.3125 Gbps (or subrate) signal input. One way to accomplish this is to use a subrate clock. For example you could try a 10.3125 Gbps / 8 = 1.2890625 GHz clock input.
Thanks,
Drew
Hi,
Apologies for the delay. Yes this is correct. The clock used to generate PRBS data is dependent on locking to a signal on the receiver.
Thanks,
Drew
Okay, I understand.
After inputting a 1.244G signal at the RX end, I am able to output a 9.953G PRBS code.
Thank you for your explanation.