This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC812R-Q1: Can maultiple device be connected on same MDIO and MDC line form Host processor.

Part Number: DP83TC812R-Q1


Hi Team,

I want to connect multiple DP83TC812R-Q1 be connected on same MDIO and MDC line form Host processor. If yes what care need to be taken and how addressing could be done form host side.

Regards

Manoj A

  • Hi Manoj, 

    This is possible. In systems with multiple PHYs using same MDIO-MDC bus, a single pull-up resistor must be used on MDIO line. It is recommended to use a resistor between 2.2 kΩ and 9 kΩ.

    You will have to strap the PHYs to different addresses. Please refer to section 8.5.3 PHY Address Configuration for the datasheet on how to do this.

    Best regards,

    Melissa