Part Number: TCA9803
Other Parts Discussed in Thread: SN74LVC1G07
My I2C controller will directly connect to about eight I2C devices. I plan on adding TCA9803 devices with port A connected to the I2C controller side and the four level shifted/isolated devices would be on port B. I would like to have VCCB controlling the EN pin, such that the device is in lowest power state when the device VCCB is not up yet. I know EN has internal pull up to VCCA. Can I tie VCCB directly to the EN pin or should I use an open-drain, non-inverting buffer between VCCB and EN.
As a side note, all TCA9803 devices VCCA will be 3.3V. The VCCB side of each device varied from 1.8V to 3.0V to 3.3V (isolation reasons). Is there any issue with this? From what the spec said, I woudl say no, but just double checking.
Thanks,
Matt