Part Number: TFP410
Hi For example, why the output of the accessory line has no image?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is /PD high or low?
Are you also providing a proper reset to the TFP410 on power-up (see section 7.4.4 of the datasheet)?
Can you measure the clock output? Please note you would need to provide external 50ohm termination to 3.3V in order to measure the clock.
Thanks
David
Hi
1. The PD is High
2. TFP410_DKEN;TFP410_MSEN;TFP410_TFADJ 10K ohm up 3V3
3. ISEL/R\E\S\E\T\ is Low i have Manul CTL High to low but same no single output
4.Can you give me reference design download link for me check my schematic TKS!!

Hi,
I do not have a TFP410 reference schematic, but looking at the schematic,

Do you see an output clock when measuring it with a scope? Please make sure the output is terminated with 50ohm termination to 3.3V.
Thanks
David