This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9544A: VOL characteristic value of PCA9544A

Guru 15160 points

Part Number: PCA9544A
Other Parts Discussed in Thread: TCA9800, TCA9544A, TCA9617A, TCA9617B

Hi, 

In the data sheet, the condition for VOL = 0.4V is IOL = 3mA, but do you have any data on the VOL characteristic value under the condition of 3mA or less?

In the current circuit configuration, VIL on the opposite side is 0.36V. We believe that if the IOL current value decreases, the VOL voltage value will decrease accordingly.

Thanks,

Conor