Part Number: TUSB322I
Other Parts Discussed in Thread: TUSB322
TUSB322I datasheet show the industrial temperature is -40~85℃,
In my use case the high working temperature of the chip on board inside the metal housing can be 95 ℃.
What's the Tj request of TUSB322I? Could it work fine in 95℃ working temperature if we make sure the calculated Tj is in range?