Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCI2050B operational current

Other Parts Discussed in Thread: PCI2050B

Team

 

My customer Shimadzu wants to know maxmum operational current of PCI2050B when both primary and secondary bus operate 33MHz with 3.3V supply. Do you have the data?

 

Best regards,

Ttesuro Shibuya

  • Hello,

    Find the power numbers on the attached file.

    Regards.

    - typ measurements are taken with 66 MHz capable SCSI card and hard drive taken behind bridge
    - Max measurements taken using bus exercisers, toggling data lines between 0 and 1.
    
    Vccp = 5V
    Vcc = 3.3V
    
    Nothing is connected to secondary bus, no primary clock:
    D0   1.2 mA  
    D1   1.2 mA  
    D2   1.2 mA  
    D3   1.2 mA  
    
    Nothing is connected to secondary bus, primary clock running at 33MHz:
    D0  29.1 mA  
    D1  29.1 mA  
    D2  10.5 mA  
    D3  10.5 mA  
    
    Nothing is connected to secondary bus, primary clock running at 66MHz:
    D0  34.1 mA  
    D1  34.1 mA  
    D2  10.5 mA  
    D3  10.5 mA  
    
    
    Conditions		Pwr State	IVcc (typ)	IVcc (max)	
    -----------------------------------------------------------------------
    Primary Bus = 33 MHz	D0		37.0 mA		169 mA		
    Secondary Bus = 33 MHz	D1		37.0 mA				
    			D2		12.4 mA				
    			D3hot		12.4 mA				
    
    Primary Bus = 66 MHz	D0		43.5 mA		189 mA		
    Secondary Bus = 33 MHz	D1		43.5 mA				
    			D2		20.7 mA				
    			D3hot		20.7 mA				
    
    Primary Bus = 66 MHz	D0		61.0 mA		234 mA		
    Secondary Bus = 66 MHz	D1		61.0 mA				
    			D2		20.5 mA				
    			D3hot		20.5 mA				

  • Thank you for your prompt answer.

     

    I would like to clarify,  does the IVcc (max) mean total current (combined both primary and secondary current)?

     

    Best regards,

    Tetsuro

     

  • Hello Tetsuro,

    It is the current consumed by the chip itself from the power supply (Vcc).

    It has nothing to do with the secondary bus.

    Regards.