Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Hi , I am planning to connect a CAN controller with transceiver (TCAN4550) to the OBD connector of a CAR. I am planning to read the engine RPM message. As I am connecting a external device, it is allowed to use a 4 meter long OBD cable and also can I connect my device without termination resistor at my device end.(If I could assume that the CAR CAN network already have two end 120 Ohm termination, Is it necessary to put a 120 ohm in my device end.