Hello, I'm Daechan Lim.
I am currently using the DP83869HM in 1000M media converter mode through strapping.
While using this chip, I have observed a phenomenon where the PHY chip goes into PWDN (power-down) mode if it fails to recognize the LINK with the MAC (Ethernet switch IC) after detecting the SD signal.
When the SD signal is detected and the SD LED illuminates, the PHY functions normally if the LINK is established within a few seconds. However, if the LINK is not recognized during the SD LED illumination for a certain period, it seems like the PHY chip goes into SLEEP mode. Even after the MAC boots up, it does not establish a connection with the PHY.
I have been unable to find information about this issue in the datasheet, and I acknowledge that there may be a possibility of a problem in my circuit design.
Does the DP83869HM go into PWDN mode when the MAC and LINK are not established?
Thank you always