Part Number: TUSB1310A
Hi,
The customer evaluation revealed that 8b/10b Decode Errors occurred when VDDA1P1 and VDD1P1=1.07 V to 1.09 V.
The recommended operating range for VDDA1P1 and VDD1P1 is 1.045 V to 1.155 V (Typ =1.1 V), but do you know what causes errors when the input voltage is below the Typ value?
Do you know the internal circuits involved in VDDA1P1 and VDD1P1?
Best Regards,
Nishie