Hi
Do i need to read the status two times to clear the INT pin if two inputs are triggered at the same time ?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is no internal queue of events. For each pin, there are two bits of state: the value when the port was read the last time, and the current value. The interrupt is active as long as the two bits are different.
Reading the port (or the input value going back to the old value) clears the interrupt.
Hi
From the datasheet, each pin I only see 1 status bit. Which register is for value read last time, and which register is for the current value ? thanks!
Hi PYTsai,
Two inputs changing state will only flag 1 interrupt since there is only one interrupt pin. 1 read of the input port register clear the interrupt. There is no internal que or buffer that stacks interrupts.
There is not a register for storing the previously recorded value. I believe any sort of memory would have to be done via software.
Regards,
Tyler