Part Number: TLIN1028-Q1
Hi,
Whether TLIN1028-Q1 can be used in slave node and backward compatible with LIN 2.1/2.0/1.3?
Thanks,
Sri Viswa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLIN1028-Q1
Hi,
Whether TLIN1028-Q1 can be used in slave node and backward compatible with LIN 2.1/2.0/1.3?
Thanks,
Sri Viswa
Hi Sri Viswa,
The FAQ above seems to suggest it should be backwards compatible.
I've assigned this thread to one of our subject matter experts who can provide further comments.
-Bobby
Hi Sri,
Sorry for the delay. Yes, TLIN1028 is compliant with all of these older LIN standards. The changes from these versions do not impact the physical layer of the LIN standard, so no updates on the transceiver-side are needed.
Let me know if you have any more questions.
Regards,
Eric Schott