Part Number: HD3SS460
Other Parts Discussed in Thread: SN65DSI86, TEST2, TPS65982, TUSB1046-DCI
For our configuration, we have our iMX8XQP driving MIPI _DSI to the eDP chip (SN65DSI86). From that chip, the 4 video lanes (ML0-ML3) and AUX_P/AUX_N are directly DC connected to the HD3SS460IR (cross point mux). From the MUX, the CSBU1 and CSBU2 lines are directly connected to our USB-C connector. The CTX1/2 lines are capacitor coupled to the USB-C connector. We are having issues getting our USB-C display module to connect and present video.
Some other MUX chips show capacitive coupling on the input of the AUX(SBU) lines.
Is our configuration correct, or do we need cap coupling on the SBU inputs on the MUX ?
Thank you