This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

device transfer RS485 to CAN



Hi team,

Could you please kindly help check if we have device to transfer RS485 to CAN?

Thanks,

Brian

  • There is no such integrated device.

    In the CAN recessive state, the differential voltage can be zero, which is not a valid RS-485 signal level. However, modern RS-485 receivers have built-in fail-safe logic that interprets an undriven bus as logic one, and a bus without such logic is supposed to have fail-safe biasing resistors with the same effect. So it might actually work to wire the buses together so that the CAN dominant state (CANH > CANL) corresponds to RS-485 logical zero (A < B).