Part Number: DP83869HM
hello
I am using a dp83869hm configured as a 1000m Media converter.
I was wondering if you could help me with a question.
1. when the SD signal is input normally, if the cupper link of the phy is not connected, LED_1 will light up and then turn off. At this time, the Cupper link is down.
In my environment, there is a 1000m Media converter using another product, and the Cupper link is connected regardless of SD (when there is no optical signal). (The chip is 88E1512 series)
I'm wondering if there is something wrong with my design or if DP83869HM works like this, but I don't have a detailed understanding of how media converters work in general.
2. 1000M MEDIA CONVERTER when using it.
If the Ethernet switch of both sides is set to AUTONEGO, should I set the setting of DP83869HM to fiber autonegotiation? Currently, I am setting it to fiber force mode, but when reconnecting the optical link, sometimes there is a suspected duplex miss match (cupper link is connected to 10M HD).
Thanks as always for your kind response.
Best regards