This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC813R-Q1: RGMII both XI and TX_CLK inputs are required?

Part Number: DP83TC813R-Q1


Hello,

In RGMII mode, I think clock input at 25MHz is required to TX_CLK pin. It seems another 25MHz clock input is necessary to XI (and XO) pin. However, in Fogure 9-4 there is no XI clock input. Does it require different 25MHz clock inputs to both TX_CLK and XI pins? Or the clock to XI can be omitted?

Thank you.

Regards,

Oguri (TIJ automotive FAE)

  • Hi Oguri-san,

    Thank you for your query. This is a typo and we shall look to correct for this in our latest revision. The PHY needs a 25MHz Reference clock at the XI pin for RGMII, as well as another 25MHz signal from the MAC to its TX_CLK.

    Sincerely,

    Gerome