Part Number: PCA9515A
Hi there,
We are attempting a similar thing to other members in thread.
We have the V-7000 DMD device on a breadboard with illumination from a 1mm square fiber connected to a laser. We are able to collimate the
light source onto DMD surface nicely (although this maybe not best practice?) The DMD is rotated at 45 degrees and the illumination is set to 24 degrees, however
the projected image is coming out at an angle. If we adjust illumination to 12 degrees it straightens up, but we think this isn't the correct angle for the illumination?
Sorry if this all sounds a bit pedestrian, but this is new territory for us. The final goal is to feed the image into an objective on the Nikon FN1 microscope.
Any help/advice would be greatly appreciated.
Mark