This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: How to confirm the eye diagram simulation is passed for FPDLINK

Part Number: DS90UB960-Q1


The camera side uses the DS90UB953

SoC side uses the DS90UB960

could you provide the eye marker? 

  • Hello Louis,

    We don't use eye mask criteria for FPD-Link III as a pass/fail criteria since measurement of the eye diagram requires shutting of the back channel from the 960 which will result in the system being in a state which doesn't match the real application. For qualification of the link between the SER/DES we recommend to verify the channel s-parameters between the pins of the SER to the pins of the DES against the channel specifications for the pair to ensure that Insertion Loss, Return Loss, and TDR are within budget as well as crosstalk (for 960 channel to channel). 

    We also have tools to show the relative system margin called MAP, which you can read about here:

    https://www.ti.com/lit/pdf/snlu243

    https://www.ti.com/lit/pdf/snla301

    Best Regards,

    Casey