Part Number: DS90UB941AS-Q1
Hi TI,
I try to check HDCP display configuration.
basically I know,
- in case of 'SoC ~ Display module' : Soc must have hdcp output logic and Display module also must, and so,
developer should certify hdcp between SoC and Display module.
- but, in case of 'SoC ~ (ser) ~ (des) ~ display' :
I wonder that, how can I configure hdcp display system.
q1. if I use SoC (which can support hdcp 1.2/1.3),
I have to make system using Ser (with HDCP) and Des IC (with HDCP)
-> I guess this can be possible system
q2. when I use SoC (which cannot support / have HDCP logic)
if I use DS90UB941 Ser and DES IC (with implement hdcp), can I say, our system can support HDCP ?
Thanks