This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: Supported wake-up behavior with TCAN1145-Q1.

Part Number: TCAN1145-Q1


Hello Expert,

I'd like to confirm TCAN1145-Q1's capability of wake-up behavior.
Our customer listed up wake up behavior as follows.

  1. Selective wake-up which is defined at ISO11898-2:2016
  2. Wake-up from WUP which is defined at ISO11898-2:2016
  3. Basic wake-up which is defined at ISO11898-2:2016

I think TCAN1145-Q1 can support 1. and 2. but it cannot support 3..
Is this understanding correct?

Best regards,
Kazuki Kuramochi

  • Hi Kuramochi-san,

    You are correct here. TCAN1145 supports wake via WUP and selective wake. The older "basic wake up" is not supported by any of our modern CAN transceivers. 

    Let me know if you have any more questions. 

    Regards, 
    Eric Schott