Part Number: SN75LVCP600S
Hi,
Can I leave the control pin open if I want a GND condition?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,
Yes if default or GND settings meets your requirement. In general, it is a good practice to use a low value Resistor - for example 1K ohm - to tie control pins to GND. This is because if there is some spikes on the GND this will protect the input.
Regards,Nasser