Other Parts Discussed in Thread: TUSB1002A, , TUSB1002, TPD4E02B04, TUSB1142, HD3SS3212, HD3SS3220
We are using TUSB1002A and TMUXHS4212I for USB3.2 gen2x1 (10Gbps) placement, and we are looking for comments on the appropriate values for AC coupling capacitors and pull-downs between each device.
*We are considering implementing 0.22uf AC coupling between TUSB1002A and TMUXHS4212I and 100Kohm pull-down on TXP/N and RXP/N, but is this okay?
TUSB1002A output (TX 22pin, 23pin) ------0.22uf—<100Kohm pulldown>----TMUXHS4212I_A0 Input
TSUB1002A input (RX 19pin, 20pin) --------0.222uf----<100Kohm pulldown>----TMUXHS4212I_A1 output
*We plan to install 0.22uF on TXp/n on the USB-C connector side of TMUXHS4212I’s B0 and C0.
Is this a stable combination for device recognition and communication on the actual machine? Also, if there are any recommended settings when combining TUSB1002A and TMUXHS4212I, could you please let me know?
Thank you in advance.